SNAU308A November 2024 – May 2025
The on-board USB2ANY interface provides a bridge between TICS Pro software and the LMX device. When the on-board USB2ANY controller is first connected to a PC, or if the firmware revision for the controller does not match with the version used by TICS Pro, a firmware update to the controller is required.
Figure 3-1 Firmware Update
Request
Figure 3-2 Firmware
Loader
Figure 3-3 Firmware Update
Complete
Figure 3-4 Connection
Mode
Figure 3-5 USB
Communications
Figure 3-6 Identify USB2ANY
Controller