SNOSDJ7A February 2025 – December 2025 LMG3650R025
PRODMIX
All faults are reported on the FLT/RDRV pin, which serves as both an input and output pin.
The FLT/RDRV is configured as an input only at the time of power-up to adjust the drive-strength, as described in Drive Strength Adjustment.
The FLT/RDRV is used as an active low digital output, indicating the fault status thereafter. The pin is a push-pull 5V digital output which goes high when all faults have cleared, which means that there is additional quiescent current through R1 when the pin is forced high.
Depending on the input threshold levels for the external digital receiver connected to the fault pin, the 1.2V step function which is forced on this pin at power-up can be interpreted as either high or low. For this reason, TI recommends that the receiver has higher thresholds such as those common for CMOS-compatible inputs and not use TTL compatible inputs. If the minimum input threshold of the external digital receiver connected to the fault pin is at or below 1.2V, the 1.2V step function at power-up can be interpreted as a high, before the LMG365xR025 is ready to begin switching.