SNOSDJ7A February 2025 – December 2025 LMG3650R025
PRODMIX
Circuits using the LMG365xR025 involve high voltage, potentially up to 650V. When laying out circuits using the LMG365xR025, understand the creepage and clearance requirements for the application and how the requirements apply to the GaN device. Functional (or working) isolation is required between the source and drain of each transistor, and between the high-voltage power supply and ground. Functional isolation or perhaps stronger isolation (such as reinforced isolation) can be required between the input circuitry to the LMG365xR025 and the power controller. Choose signal isolators and PCB spacing (creepage and clearance) distances which meet the user-specific isolation requirements.
If a heat sink is used to manage thermal dissipation of the LMG365xR025, establish that necessary electrical isolation and mechanical spacing is maintained between the heat sink and the PCB.