SPRAD14 April   2022 AM67 , AM67A , AM68 , AM68A , AM69 , AM69A , DRA821U , DRA821U-Q1 , DRA829J , DRA829J-Q1 , DRA829V , DRA829V-Q1 , TDA4AEN-Q1 , TDA4AH-Q1 , TDA4AL-Q1 , TDA4AP-Q1 , TDA4APE-Q1 , TDA4VE-Q1 , TDA4VEN-Q1 , TDA4VH-Q1 , TDA4VL-Q1 , TDA4VM , TDA4VM-Q1 , TDA4VP-Q1 , TDA4VPE-Q1

 

  1.   Trademarks
  2. 1Introduction
  3. 2Dual TDA4 System
    1. 2.1 Dual TDA4x SoC System Diagram
    2. 2.2 System Consideration and BOM Optimization
  4. 3Camera Connection
    1. 3.1 Duplicate Front Camera Input to Two TDA4x SoCs
    2. 3.2 Connect Front Camera to Only one TDA4x
  5. 4Boot Sequence Solution
    1. 4.1 Boot Solution Based on Dual Flash
    2. 4.2 Boot Solution Based on Single Flash
  6. 5Multi-SoC Demo Based on PCIe
  7. 6References

Duplicate Front Camera Input to Two TDA4x SoCs

This solution duplicates the camera source data to two TDA4x SoCs, (TDA4-A, TDA4-B) each TDA4x processor implements different ADAS functions. A reference implementation to distribute front camera functionality, as shown in Figure 3-1.

Figure 3-1 Typical Camera Duplicate Solution

Camera in Primary TDA4-A:

  • Front camera is used to monitor the front camera object:
    • The camera data input through CSI2-1 port
    • Preprocessing by C66x DSP (such as Format/Grayscale conversion, ROI Setting)
    • Run inference on deep learning models to achieve Lane Departure Warning (LDW) and Lane Keeping Assist (LKA) function in C7x+MMA deep learning accelerator
    • Postprocessing by C66x DSP (such as drawing line and interpolation) and output the result to fusion node
  • Side view cameras are used to monitor car and objects coming from the side:
    • The camera data input through CSI2-0 port
    • Preprocessing/postprocessing by C66x DSP
    • Run inference on deep learning models for Lane Changing Assist (LCA) and Adaptive Cruise Control (ACC) in C7x+MMA
    • Output the result to fusion node

Camera in Secondary TDA4-B:

  • Front camera is used to monitor the front object:
    • The camera data input through CSI2-0 port
    • Preprocessing/postprocessing is done by C66x DSP
    • Run inference deep learning models to achieve Object Detect (OD) function in C7x+MMA, such as Traffic Light Recognition (TLR), Traffic Sign Recognition (TSR)
    • Output the result to PCIe TX node
  • Surround view cameras are used to detect the environment around the car at low speed:
    • The camera data input through CSI2-1 port
    • The codec node is optional for recording (DVR)
    • GPU node for 3D rendering
    • Preprocessing/postprocessing by C66x DSP
    • Run inference deep learning models to achieve Automated Valet Parking (AVP) and Automated Parking Assist (APA) function in C7x+MMA
    • Output the result to PCIe TX node

Fusion:

  • All of the results from the TDA4-B are transferred to the TDA4-A via PCIe TX/RX node, then input to fusion node.
  • All of the results whether from TDA4-A or TDA4-B are assembled in fusion node, then output the finally result.