SPRUJF8 May 2026 TMS320F28P551SD , TMS320F28P551SG
FILE: lin_ex1_loopback_interrupts.c
This example configures the LIN module in commander mode for internal loopback with interrupts. The module is setup to perform 8 data transmissions with different transmit IDs and varying transmit data. Upon reception of an ID header, an interrupt is triggered on line 0 and an interrupt service routine (ISR) is called. The received data is then checked for accuracy.
The example can be adjusted to use interrupt line 1 instead of line 0 by un-commenting "LIN_setInterruptLevel1()"
External Connections
Watch Variables