SPRUJF8 May 2026 TMS320F28P551SD , TMS320F28P551SG
The control law accelerator can be programmed in either CLA assembly code, using the instructions described in Section 7.7, or a reduced subset of the C language. CLA assembly code resides in the same project with C28x code. The only restriction is the CLA code must be in the assembly section. This can be easily done using the .sect assembly directive. This does not prevent CLA and C28x code from being linked into the same memory region in the linker command file.
System and CLA initialization are performed by the main CPU. This can typically be done in C or C++ but can also include C28x assembly code. The main CPU also copies the CLA code to the program memory and, if needed, initialize the CLA data RAMs. Once system initialization is complete and the application begins, the CLA services the interrupts using the CLA assembly code (or tasks). The main CPU can perform other tasks concurrently with CLA program execution.