SPRUJF8 May 2026 TMS320F28P551SD , TMS320F28P551SG
To migrate an existing application that is configured to run from RAM to a Flash-based linker configuration, follow these steps:
device_support\<device>\common\cmd
directory.BEGIN in TI-provided Flash linker
command files) at the end of boot code execution. Make sure there is a
branch instruction at the Flash entry point to your code initialization (for
example, _c_int00) function. In the C2000Ware examples, the
entry point code is specified in the codestartbranch.asm
file.Flash_initModule() driverlib function achieves these
steps. Note that code that initializes the Flash module must execute from a
RAM location. This is accomplished by assigning the Flash initialization
function to the .TI.ramfunc section. In the linker command
file, map this section to Flash for load, and RAM for execution. The example
cmd files provided in the C2000Ware show how to do
this correctly..TI.ramfunc section in the TI-provided Flash linker
command files accomplishes this purpose.ALIGN directive in the linker command file.type=NOINIT") in the linker command
file.