SPRUJF8 May 2026 TMS320F28P551SD , TMS320F28P551SG
FILE: erad_ex2_profilefunction.c
This example contains a basic FIR calculation and sorting algorithm to help demonstrate the function profiling capability of the ERAD peripheral. A number of FIR sums are calculated within a loop and are then sorted using the insertion sort algorithm. Cycle counts of both the FIR calculations and the sorting algorithm are output to the screen through the scripting console. In this example, it can be seen that sorting the data takes up a majority of the CPU cycles executed in this program.
To properly use the provided ERAD script, the following variables must be set in the scripting environment prior to launching the ERAD script:
The included JavaScript file, erad_ex2_profile_function.js, uses Debug Server Scripting (DSS) features. For information on using the DSS, please visit: http://software-dl.ti.com/ccs/esd/documents/users_guide/sdto_dss_handbook.html
This example uses 4 HW breakpoints and 2 counters:
External Connections
Watch Variables
Profiling Script Output
Note that the the counters are reset after the stop event. The counter value remains 0 till the next start event occurs. The javascript continuously reads the counter value in a while(1) and hence the current counter may return 0.