SPRUJF8 May 2026 TMS320F28P551SD , TMS320F28P551SG
The Rx FIFO overwrite mode is configured by MCAN_RXFnC[31].FnOM = 1. When an Rx FIFO full condition is reached (MCAN_RXFnS[21:16].FnPI = MCAN_RXFnS[13:8].FnGI) signaled by MCAN_RXFnS[24].FnF = 1, the next accepted message for the FIFO overwrites the oldest FIFO message. Put index/Get index are both incremented by one.
In overwrite mode if an Rx FIFO full condition is signaled, reading of the Rx FIFO elements starts at least at get index + 1. The reason for this is a received message is written to the Message RAM (Put index) while the Host CPU is reading from the Message RAM (Get index). In this case, inconsistent data can be read from the respective Rx FIFO element. The problem is solved by adding an offset to the Get index when reading from the Rx FIFO. The offset depends on how fast the Host CPU accesses the Rx FIFO. Figure 27-16 shows an offset of two with respect to the Get index when reading the Rx FIFO. In this case, the two messages stored in element 1 and 2 are lost.
After reading from the Rx FIFO, the number of the last element read has to be written to the Rx FIFO Acknowledge Index MCAN_RXFnA[5:0].FnAI. This increments the get index to that element number. In case the Put index has not been incremented to this Rx FIFO element, the Rx FIFO full condition is reset (MCAN_RXFnS[24].FnF = 0).
Figure 27-16 Rx FIFO Overflow Handling