SPRUJF8 May 2026 TMS320F28P551SD , TMS320F28P551SG
The CPU Secure Logic (CPUSL) on this device prevents a hacker from reading the CPU registers in a CCS watch window while code is running in a secure zone. All accesses to CPU registers when the PC points to a secure location are blocked by this logic. The only exception to this is read access to the PC. It is highly recommended not to write into the CPU register in this case, because proper code execution may get affected. If the CSM is unlocked using the CSM PMF, the CPUSL logic also gets disabled.