SPRUJ53 April 2024 TMS320F28P550SJ , TMS320F28P559SJ-Q1
There are two ECC blocks (ECC64_H and ECC64_L) inside the Flash Read Interface. These ECC blocks correct single-bit Flash read errors, and can detect uncorrectable errors of two or more bits. The ECC blocks are also capable of detecting address errors. The ECC blocks operate using eight user-calculated ECC check bits associated with each 64-bit wide data word and the corresponding 128-bit memory-aligned address. Users must program these ECC check bits into ECC memory space, along with Flash data during the Flash programming operation. Refer to the device data sheet for the Flash/OTP ECC memory-map.
The ECC bits for a given Flash address and 64-bit data word can be calculated using the Flash API; however, TI recommends using the AutoEccGeneration option available in the Flash Plugin or API to auto-calculated and program ECC bits. The Flash API uses hardware ECC logic in the device to generate the ECC data for the given Flash data. The Flash Plugin, the Flash programming tool integrated with the Code Composer Studio™ IDE, uses the Flash API to generate and program ECC data.
Figure 6-3 illustrates the ECC logic inputs and outputs.
During an instruction fetch or a data read operation, the 19 most-significant address bits (the three least-significant bits of address are not considered), together with the 64-bit data/8-bit ECC read-out of Flash banks/ECC memory-map area, pass through the ECC logic, and the eight check bits are produced in ECC block. These eight calculated ECC check bits are then XORed with the stored check bits (user programmed check bits) associated with the address and the read data. The 8-bit output is decoded inside the ECC block to determine one of three conditions:
A single-bit error in the address field is considered to be a non-correctable error.
The ECC feature is enabled by default at reset, and can be enabled or disabled by writing to the ECC_ENABLE register. ECC logic is automatically bypassed when the 64 data bits and associated ECC bits fetched from the bank are either all ones or all zeros.