DLPU140A May 2024 – September 2025 DLP160AP , DLP160CP , DLP2000 , DLP2010 , DLP2010LC , DLP2010NIR , DLP2021-Q1 , DLP230GP , DLP230KP , DLP230NP , DLP300S , DLP3010 , DLP3010LC , DLP301S , DLP3020-Q1 , DLP3021-Q1 , DLP3030-Q1 , DLP3034-Q1 , DLP3310 , DLP4500 , DLP4500NIR , DLP4620S-Q1 , DLP4621-Q1 , DLP470NE , DLP470TE , DLP4710 , DLP4710LC , DLP471NE , DLP471TE , DLP471TP , DLP480RE , DLP500YX , DLP5500 , DLP550HE , DLP550JE , DLP5530-Q1 , DLP5530S-Q1 , DLP5531-Q1 , DLP5531A-Q1 , DLP5532-Q1 , DLP5533A-Q1 , DLP5534-Q1 , DLP6500FLQ , DLP6500FYE , DLP650LE , DLP650LNIR , DLP650NE , DLP650TE , DLP651LE , DLP651NE , DLP660TE , DLP670RE , DLP670S , DLP7000 , DLP7000UV , DLP780NE , DLP780TE , DLP781NE , DLP781TE , DLP800RE , DLP801RE , DLP801XE , DLP9000 , DLP9000X , DLP9000XUV , DLP9500 , DLP9500UV
These fields are not user inputs. The output gives the calculated average diffraction efficiency and average photopic diffraction efficiency. The average diffraction efficiency is calculated by taking an average of the diffraction efficiency values across the specified wavelength spectrum. The photopic diffraction efficiency is taken by multiplying the diffraction efficiency with the normalized photopic response at the corresponding wavelengths. This is done as a summation taken across the entire wavelength spectrum. The result is then divided by the summation of the photopic response values across the wavelength spectrum.
S (λi) is the source spectrum and Phot (λi) is the photopic curve. The average is then taken across the spectrum to show the value displayed in the application.
Figure 3-8 Diffraction pattern. Light
inside the dotted blue line is collected by the projection optics. Light outside
the dotted blue line is lost in diffraction lobes. Diffraction efficiency is
light collected divided by total light.