SCPS286 July 2025 TPLD2001
ADVANCE INFORMATION
Combinationial logic is supported via Look-up Tables (LUTs) within the TPLD2001. Inputs and outputs for the combination function macro-cells are configured from the connection mux with specific logic functions being defined by the state of OTP bits.
The TPLD2001 has sixteen configurable use logic blocks (macro-cells) that can serve as a combinational or sequential logic function. In each case, they can serve as a Look-up Table (LUT), or as another logic or timing function. See the list below for the functions that can be implemented in these logic blocks:
One selectable 2-input LUT or pattern generator (PGEN)
Four selectable 3-input LUT or DFF/L or Shift register (SR)