SLVA477C December   2011  – September 2026 TLV62080 , TLV62085 , TLV62090 , TLV62130 , TLV62130A , TLV62150 , TLV62150A , TPS62000 , TPS62000-HT , TPS62002 , TPS62003 , TPS62004 , TPS62005 , TPS62006 , TPS62007 , TPS62008 , TPS62020 , TPS62021 , TPS62026 , TPS62040 , TPS62042 , TPS62043 , TPS62044 , TPS62046 , TPS62050 , TPS62051 , TPS62052 , TPS62054 , TPS62056 , TPS62060 , TPS62061 , TPS62063 , TPS62065 , TPS62067 , TPS62080 , TPS62080A , TPS62081 , TPS62082 , TPS62085 , TPS62086 , TPS62087 , TPS62088 , TPS62090 , TPS62090-Q1 , TPS62091 , TPS62092 , TPS62093 , TPS62097 , TPS62097-Q1 , TPS62100 , TPS62101 , TPS62102 , TPS62103 , TPS62110 , TPS62110-EP , TPS62110-HT , TPS62110-Q1 , TPS62111 , TPS62111-EP , TPS62112 , TPS62112-EP , TPS62113 , TPS62120 , TPS62122 , TPS62125 , TPS62130 , TPS62130A , TPS62131 , TPS62132 , TPS62133 , TPS62135 , TPS62136 , TPS62140 , TPS62140A , TPS62141 , TPS62142 , TPS62143 , TPS62150 , TPS62150A , TPS62151 , TPS62152 , TPS62153 , TPS62160 , TPS62161 , TPS62162 , TPS62163 , TPS62170 , TPS62171 , TPS62172 , TPS62173 , TPS62175 , TPS62177 , TPS62180 , TPS62200 , TPS62201 , TPS62202 , TPS62203 , TPS62204 , TPS62205 , TPS62207 , TPS62208 , TPS62220 , TPS62221 , TPS62222 , TPS62223 , TPS62224 , TPS62225 , TPS62227 , TPS62228 , TPS62230 , TPS62231-Q1 , TPS622314-Q1 , TPS62240 , TPS62242 , TPS62242-Q1 , TPS62243 , TPS62250 , TPS62260 , TPS62260-Q1 , TPS62261 , TPS62261-Q1 , TPS62262 , TPS62262-Q1 , TPS62263 , TPS62263-Q1 , TPS62270 , TPS62272 , TPS62273 , TPS62290 , TPS62290-Q1 , TPS62291 , TPS62293 , TPS62293-Q1 , TPS62300 , TPS62301 , TPS62302 , TPS62303 , TPS62304 , TPS62305 , TPS62320 , TPS62321 , TPS62350 , TPS62352 , TPS62353 , TPS62354 , TPS62355 , TPS62356 , TPS62360 , TPS62361B , TPS62362 , TPS62363 , TPS62366A , TPS62366B , TPS62400 , TPS62400-Q1 , TPS62401 , TPS62402 , TPS62402-Q1 , TPS62403 , TPS62404 , TPS62404-Q1 , TPS62406-Q1 , TPS62407-Q1 , TPS62410 , TPS62410-Q1 , TPS62420 , TPS62420-Q1 , TPS62421 , TPS62422-Q1 , TPS62423-Q1 , TPS62424-Q1 , TPS62510 , TPS62560 , TPS62561 , TPS62562 , TPS62590 , TPS62590-Q1 , TPS62601 , TPS62612 , TPS62615 , TPS62616 , TPS62619 , TPS62620 , TPS62621 , TPS62622 , TPS62623 , TPS62624 , TPS62625 , TPS62650 , TPS62650-Q1 , TPS62651 , TPS62660 , TPS62665 , TPS62671 , TPS62672 , TPS62674 , TPS62675 , TPS62679 , TPS62690 , TPS62693 , TPS62700 , TPS62730 , TPS62732 , TPS62733 , TPS62740 , TPS62750 , TPS62751 , TPS62800 , TPS62801 , TPS62802 , TPS62806 , TPS62807 , TPS62808 , TPS62821 , TPS62822 , TPS62823 , TPS62825 , TPS62826 , TPS62840 , TPS62870 , TPS62870-Q1 , TPS62871 , TPS62871-Q1 , TPS62872 , TPS62872-Q1 , TPS62873 , TPS62873-Q1 , TPS62874-Q1 , TPS62875-Q1 , TPS62876-Q1 , TPS62877-Q1 , TPS65000 , TPS65001 , TPS65010 , TPS65011 , TPS65012 , TPS65013 , TPS65014 , TPS65020 , TPS65021 , TPS65022 , TPS65023 , TPS650231 , TPS65050 , TPS65055 , TPS65070 , TPS65072 , TPS65073 , TPS650830 , TPS65086 , TPS65090 , TPS65137 , TPS65160 , TPS65160A , TPS65161 , TPS65161A , TPS65161B , TPS65162 , TPS65163 , TPS65167A , TPS65175 , TPS65175B , TPS65175C , TPS65177 , TPS65177A , TPS65180B , TPS65181B , TPS65182B , TPS65217 , TPS65218 , TPS65218D0 , TPS65640 , TPS65642 , TPS65642A , TPS65720 , TPS65721 , TPS65910 , TPS65911 , TPS65912 , TPSM8287A06 , TPSM8287A10 , TPSM8287A12 , TPSM8287A15 , TPSM8287B15 , TPSM8287B30

 

  1.   1
  2.   Abstract
  3. 1Basic Configuration of a Buck Converter
    1. 1.1 Necessary Parameters of the Power Stage
  4. 2Calculate the Maximum Switch Current
  5. 3Inductor Selection
  6. 4Rectifier Diode Selection
  7. 5Output Voltage Setting
  8. 6Input Capacitor Selection
  9. 7Output Capacitor Selection
  10. 8References
  11. 9Revision History
  12.   A Formulas to Calculate the Power State of a Buck Converter

Calculate the Maximum Switch Current

The first step to calculate the switch current is to determine the duty cycle, D, for the maximum input voltage. The maximum input voltage is used because this leads to the maximum switch current.

Equation 1. TLV62080

VIN(max) = maximum input voltage
VOUT = output voltage
η = efficiency of the converter, e.g., estimated 90%

The efficiency is added to the duty cycle calculation, because the converter also has to deliver the energy dissipated. This calculation gives a more realistic duty cycle than just the formula without the efficiency factor.

Use either an estimated factor, e.g., 90% (which is not unrealistic for a buck converter worst-case efficiency), or see the Typical Characteristics section of the data sheet of the selected converter.

The next step in calculating the maximum switch current is to determine the inductor ripple current. In the converter's data sheet; normally, a specific inductor or a range of inductors are named for use with the IC. So, use the recommended inductor value to calculate the ripple current, an inductor value in the middle of the recommended range, or if none is given in the data sheet, the one calculated in the Inductor Selection section of this application report.

Equation 2. TLV62080

VIN(max) = maximum input voltage
VOUT = desired output voltage
D = duty cycle calculated in Equation 1
fS = minimum switching frequency of the converter
L = selected inductor value

It now has to be determined if the selected IC can deliver the maximum output current.

Equation 3. TLV62080

ILIM(min) = minimum value of the current limit of the integrated switch (given in the data sheet)
ΔIL = inductor ripple current calculated in Equation 2

If the calculated value for the maximum output current of the selected IC, IMAXOUT, is below the system's required maximum output current, the switching frequency has to be increased to reduce the ripple current or another IC with a higher switch current limit has to be used.

Only if the calculated value for IMAXOUT is just a little smaller than the needed one, it is possible to use the selected IC with an inductor with higher inductance if it is still in the recommended range. A higher inductance reduces the ripple current and therefore increases the maximum output current with the selected IC.

If the calculated value is above the maximum output current of the application, the maximum switch current in the system is calculated:

Equation 4. TLV62080

ΔIL = inductor ripple current calculated in Equation 2
IOUT(max) = maximum output current necessary in the application

This is the peak current, the inductor, the integrated switch(es), and the external diode have to withstand.