SPRACM3E August   2021  – January 2023 F29H850DM , F29H850DU , F29H850TU , F29H859TU-Q1 , F29P329SM-Q1 , F29P580DM , F29P589DM-Q1 , F29P589DU-Q1 , TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1 , TMS320F28384D , TMS320F28384S , TMS320F28386D , TMS320F28386S , TMS320F28388D , TMS320F28388S , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1

 

  1.   Using the Fast Serial Interface (FSI) With Multiple Devices in an Application
  2.   Trademarks
  3. 1Introduction to the FSI Module
  4. 2FSI Applications
  5. 3Handshake Mechanism
    1. 3.1 Daisy-Chain Handshake Mechanism
    2. 3.2 Star Handshake Mechanism
  6. 4Sending and Receiving FSI Data Frames
    1. 4.1 FSI Data Frame Configuration APIs
    2. 4.2 Start Transmitting Data Frames
  7. 5Daisy-Chain Topology Tests
    1. 5.1 Two Device FSI Communication
      1. 5.1.1 CPU Control
      2. 5.1.2 DMA Control
      3. 5.1.3 Hardware Control
    2. 5.2 Three Device FSI Communication
      1. 5.2.1 CPU/DMA Control
      2. 5.2.2 Hardware Control
        1. 5.2.2.1 Skew Compensation for Three Device Daisy-Chain System
          1. 5.2.2.1.1 CPU/DMA control
          2. 5.2.2.1.2 Hardware Control
  8. 6Star Topology Tests
  9. 7Event Synchronization Over FSI
    1. 7.1 Introduction
      1. 7.1.1 Requirement of Event Sync for Distributed Systems
      2. 7.1.2 Solution Using FSI Event Sync Mechanism
      3. 7.1.3 Functional Overview of FSI Event Sync Mechanism
    2. 7.2 C2000Ware FSI EPWM Sync Examples
      1. 7.2.1 Location of the C2000Ware Example Project
      2. 7.2.2 Summary of Software Configurations
        1. 7.2.2.1 Lead Device Configuration
        2. 7.2.2.2 Node Device Configuration
      3. 7.2.3 1 Lead and 2 Node F28002x Device Daisy-Chain Tests
        1. 7.2.3.1 Hardware Setup and Configurations
        2. 7.2.3.2 Experimental Results
      4. 7.2.4 1 Lead and 8 Node F28002x Device Daisy-Chain Tests
        1. 7.2.4.1 Hardware Setup and Configurations
        2. 7.2.4.2 Experimental Results
      5. 7.2.5 Theoretical C2000 Uncertainties
    3. 7.3 Additional Tips and Usage of FSI Event Sync
      1. 7.3.1 Running the Example
      2. 7.3.2 Target Configuration File
      3. 7.3.3 Usage of Event Sync for Star Configuration
  10. 8References
  11. 9Revision History

Hardware Setup and Configurations

The provided daisy-chain example is run on 1 lead LAUNCHXL-F280025C device with 2 node LAUNCHXL-F280025C devices along with TMDSFSIADAPEVM boards with each lead and node devices. The devices are connected using a cable with length of 1ft. The operating PWM frequency has been considered at 20kHz with 50% duty ratio. The FSI clock is configured to operate at 50MHz. The CLB counter ‘match’ values as per the calculation of Node 1 having 43*(N-1) will have ‘match’ value as 43 and Node 2 will have value as 1.

Figure 7-8 1 Lead - 2 Node Device Setup