SPRADJ0 February 2025 AM2612 , AM2612-Q1 , AM2631 , AM2632 , AM2634 , AM263P2 , AM263P4 , AM2732 , AM2732-Q1 , AM620-Q1 , AM623 , AM625 , AM625-Q1 , AM62A3 , AM62A3-Q1 , AM62A7 , AM62A7-Q1 , AM62D-Q1 , AM62P , AM62P-Q1 , AM67 , AM68A , AM69A , DRA821U , TDA4AEN-Q1 , TDA4AH-Q1 , TDA4AL-Q1 , TDA4AP-Q1 , TDA4VE-Q1 , TDA4VEN-Q1 , TDA4VH-Q1 , TDA4VL-Q1 , TDA4VM , TDA4VP-Q1
Examples of make syntax are provided in the following:
make [-s] <build_target> [BOARD=<device_evm_name>] [SOC=<soc_name>] [SDK_INSTALL_PATH=<sdk_install_path>] [PROFILE=<release/debug>] ...
make [-s] <build_target> [PLATFORM=<soc_name>] [PROFILE=<release/debug>] ...
Figure 3-1 shows a Microsoft Windows 11 example where the gmake -s adc_app
command builds the ADC application along with the driver sources from the
gmake dependencies.
Figure 3-1 Make Output Example