SPRADJ6 November   2026 AWR1243 , AWR1443 , AWR1642 , AWR1843 , AWR2188 , AWR2243 , AWR2544 , AWR2944 , AWR2944P , AWR6443 , AWR6843 , AWRL1432 , AWRL6432 , AWRL6844 , AWRL6888 , IWR1443 , IWR1642 , IWR1843 , IWR2188 , IWR2243 , IWR2944 , IWR6243 , IWR6443 , IWR6843 , IWRL1432 , IWRL6432 , IWRL6432W , IWRL6843 , IWRL6844

 

  1.   1
  2.   Abstract
  3. 1Introduction
    1. 1.1 What is a mmWave Radar Antenna?
    2. 1.2 Features of mmWave Radar Antennas
      1. 1.2.1 Fundamental Antenna Parameters
      2. 1.2.2 Fundamental Antenna Array Parameters
    3. 1.3 Antenna Type Selection
    4. 1.4 Critical Sections of Antenna
      1. 1.4.1 Source
      2. 1.4.2 Feeding Network
      3. 1.4.3 Radiating Element
    5. 1.5 Antenna Array and Pattern Selection
      1. 1.5.1 Virtual Antenna Array
    6. 1.6 PCB Material Impact on Antenna Performance
  4. 2Antenna Design Flow
    1. 2.1 End Application Evaluation
    2. 2.2 Form Factor and Stack-up Decision
    3. 2.3 Link Budget and Antenna Feature Definition
    4. 2.4 Single Antenna Element Design
    5. 2.5 Antenna Array Design
    6. 2.6 Layout Creation and Simulation
    7. 2.7 Fabrication and Design Validation
  5. 3Summary
  6. 4References

Form Factor and Stack-up Decision

The form factor of a radar sensor board depends on the application, and it limits how much space the antennas can occupy. An automotive door-handle sensor, for example, must fit inside the handle, which sets a tight size limit. The stack-up (substrate, layer count, copper type) is decided together with the form factor, because the two together determine what antenna performance is achievable.

Impact of Form Factor on Antenna Design

  • Number of elements and angular resolution: A small board limits the area for TX and RX arrays. Fewer elements mean a smaller virtual aperture, which reduces angular resolution.
  • Element spacing: The RX spacing (typically λ/2) and the TX spacing needed to build the virtual array must fit within the available area. Tight space may force compromises in spacing and layout.
  • Array size and gain: The antenna size and the number of patches in each array are limited, so gain is limited too. Fitting multiple patches and the feed network for higher gain becomes difficult.
  • TX–RX isolation: Placing the TX and RX arrays close together increases coupling through surface waves, substrate modes, and direct radiation leakage. This raises the leakage into the receiver, which can reduce sensitivity. Isolation can be improved with via fences, ground slots, or absorber and shielding structures, and by orienting the arrays carefully, though these use additional space.
  • Routing and components: The same area must hold the radar IC, feed lines, power circuitry, and connectors, so the antenna area competes with the rest of the board.
  • Radome and enclosure: A tight enclosure places the radome close to the antenna, which can detune the patches, shift the pattern, and add loss. The radome thickness and distance should be considered at this stage.

Stack-up Decision

  • Substrate selection: Choose the dielectric material based on the application's performance needs and cost limits (Dk, Df, thickness, stability), as discussed in Step 1.
  • Layer count: More layers allow compact routing and options such as aperture or proximity coupling, but they add cost.
  • Hybrid stack-up: A low-loss laminate for the top RF layer with standard FR-4 for the rest balances performance and cost.
  • Copper type and surface finish: These are selected to keep conductor loss low at mmWave.
  • Thickness: Substrate thickness affects bandwidth, surface waves, and the line widths needed for impedance control.
  • Cost Considerations: A smaller board uses less PCB material, which reduces cost. However, a compact design may need a better laminate, more layers, or tighter fabrication tolerances to reach the required performance, which can offset those savings. The cost impact should therefore be judged for the whole design, not just the board area.
  • Manufacturability: The fabrication tool limitations set limits to the minimum manufacturable dimension of copper traces and via drills. Etching tolerances and layer thickness tolerances also add up to the manufacturing variations.

Design Example

The board design is targeted for a very low form factor with dimensions 36mm x 24mm as the mounting space on the vehicle rear bumper is limited and this is a very low cost solution. The antenna design area is confined by this size.

The board layer stack-up with layer counts is shown in Table 2-1.The RF material used here is Isola FR408HR which is one of the cheapest materials available in the market. It has a Dk of approximately 3.26 and Df of approximaately 0.02 at 76-81GHz, and 5 mil thickness. The number of stack-up layers have been restricted to four to reduce the cost of PCB.

Table 2-1 Layer Stack-up
Layer Name Material Thickness Dk
Top Solder Solder Resist 0.80mil 1
1 Top Layer Copper 1.60mil
Dielectric 1 ISOLA FR408HR DUAL PLY, 2x1067, SPREAD GLASS 5mil 3.26
2 L2_GND Copper 1.40mil
Dielectric 2 PCL370HR 45mil 4
3 L3_SIG Copper 1.40mil
Dielectric 3 PCL370HR 5mil 4
4 Bottom Layer Copper 1.60mil
Bottom Solder Solder Resist 0.80mil 1