SPRADJ6 November 2026 AWR1243 , AWR1443 , AWR1642 , AWR1843 , AWR2188 , AWR2243 , AWR2544 , AWR2944 , AWR2944P , AWR6443 , AWR6843 , AWRL1432 , AWRL6432 , AWRL6844 , AWRL6888 , IWR1443 , IWR1642 , IWR1843 , IWR2188 , IWR2243 , IWR2944 , IWR6243 , IWR6443 , IWR6843 , IWRL1432 , IWRL6432 , IWRL6432W , IWRL6843 , IWRL6844
Selecting an antenna involves balancing several factors: the target application, the operating frequency, the available form factor, ease of manufacture, and overall cost. The application is the starting point, because it defines what the antenna must deliver in gain, directivity, bandwidth, and FOV.
Consider a satellite communication link. It requires a highly directive antenna with high gain and a narrow FOV so that energy is focused toward a distant target. Size is a secondary concern in such systems, so physically large antennas such as Yagi-Uda, horn, and helical designs are common. These structures typically operate at lower frequencies, where their larger dimensions are practical.
mmWave applications present a different set of constraints. At these frequencies, wavelengths are only a few millimeters, and the antenna must fit within compact devices. The form factor is therefore dictated by both the application and the operating frequency. Several antenna types can be realized at this small scale, including dipoles, monopoles, and patches. The final choice depends mainly on the required radiation pattern. Dipole and monopole antennas, for example, provide omnidirectional coverage, radiating roughly equally in all directions. That is useful for general connectivity but less suited to sensing, where controlled coverage is usually needed.
Why Patch Antennas Are Preferred for mmWave Radar
Patch antennas have become the dominant choice for mmWave radar sensor boards, for several reasons.
A patch antenna is built from a dielectric substrate sandwiched between two copper layers. The radiating element is formed on the top layer by etching away unwanted copper, leaving a patch of defined shape and dimensions. The bottom copper layer remains intact and serves as the reference ground plane. This design is shown in Figure 1-7
A single patch provides moderate gain with a relatively wide beam. When a radar needs longer range, multiple patches are arranged in an array. Their combined radiation increases gain and produces a more directive beam. This comes at the cost of a narrower FOV, so the array size and layout must be chosen to strike the right balance between range and coverage for the application.
Figure 1-7 Microstrip Patch
Antenna