SPRT759 October 2023 TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1 , TMS320F28075 , TMS320F28075-Q1 , TMS320F28076 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377D-EP , TMS320F28377D-Q1 , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28378D , TMS320F28378S , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S , TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
Table 5-2 is a summary of Unique IDs referenced in this section. For further details, see the device-specific Functional Safety Manual.
Unique ID | Short Description | Notes / Software Support |
---|---|---|
ADC2 | DAC to ADC loopback check | |
ADC8 | ADC input signal integrity check | |
ADC10 | Hardware redundancy | |
CAN3 | SRAM Parity | |
CLA1 | Software reciprocal comparison | |
CLA2 | Software test of CPU | CLA_STL |
CLA3 | Handling of illegal operation and illegal results | |
CLK2 | Integrity using CPU timer | SDL module: STL_OSC_CT |
CLK3 | Integrity using HRPWM | SDL module: STL_OSC_HR |
CLK4 | Dual clock comparator (DCC type0) | |
CLK16 | Dual clock comparator (DCC type1) | Note: DCC type 1 is identical to type 2. |
CLK17 | Dual clock comparator (DCC type2) | |
CPU1 | Software reciprocal comparison | |
CPU2 | Hardware built-in test of CPU | SDL module: STL_HWBIST |
CPU3 | Software test of CPU | C28X_STL |
CPU7 | Handling of illegal operation, illegal results and instruction trapping | |
DCSM2 | Majority voting and error detection of link pointer | |
ECAT6 | SRAM parity | |
EFUSE2 | EFUSE ECC (data only) | |
FLASH1 | Flash ECC (data + address) | |
FLASH2 | VCU CRC check of memory | SDL module: STL_CRC |
FLASH6 | Software test of ECC logic | SDL modules: sdl_ex_ram_ecc_parity_test and sdl_ex_flash_ecc_test |
GPIO4 | Software test of function using I/O loopback | |
GPIO5 | Hardware redundancy | |
INC1 | Software test of function including error tests | |
INC8 | Transmission redundancy | |
INC9 | Hardware redundancy | |
MCAN8 | SRAM ECC (data + address) | |
PIE1 | PIE double SDRAM hardware comparison | |
PIE2 | Software test of SRAM | |
PIE3 | Software test of ePIE including error tests | |
PIE6 | PIE double SRAM comparison check | SDL module: STL_PIE_RAM |
PIE8 | Online monitoring of interrupts and events | |
PIE13 | Hardware redundancy using lockstep compare | |
ROM1 | VCU CRC check of memory | SDL module: STL_CRC |
ROM9 | Background CRC for CLA program ROM | |
ROM10 | Memory power-on Self-test (MPOST) | |
ROM15 | ROM parity | |
SRAM1 | SRAM ECC (data + address) | |
SRAM2 | SRAM Parity | |
SRAM3 | Software test of SRAM | SDL module: STL_March |
SRAM8 | VCU CRC check of memory | SDL module: STL_CRC |
SRAM14 | Software test of parity logic | SDL modules: sdl_ex_ram_ecc_parity_test |
STL_CPU_REG | CPU register test example from the diagnostic library | For a device that does not include HWBIST, a periodic test of the CPU registers can be performed. STL_CPU_REG does not map to a C2000 Unique ID directly. STL_CPU_REG refers to an example CPU register test within the diagnostic library. This example is also provided for other devices if needed. Refer to the diagnostic library documentation. |