SPRT759 October 2023 TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1 , TMS320F28075 , TMS320F28075-Q1 , TMS320F28076 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377D-EP , TMS320F28377D-Q1 , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28378D , TMS320F28378S , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S , TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
Terminology and Abbreviations | Definition |
---|---|
A.x... | Reference from the UL 1998 standard. For example: A.7.1.19 is a specific definition found in appendix A of the standard. |
C28x | A C2000 central processing unit. |
CLA | C2000 Control Law Accelerator: an independent 32-bit floating-point processor. |
CLA PROM | Program ROM for the CLA CPU |
CLB | C2000 Configurable Logic Block |
Class B / 1 | IEC 60730 Class B and UL 1998 Class 1. Class assigned based on a functional safety assessment. Refer to c. |
Class C / 2 | IEC 60730 Class C and UL 1998 Class 2: Class assigned based on a functional safety assessment. Refer to Table 2-1. |
CLK | Clock |
CPU | Central Processing Unit |
CPU Timer | C2000 general timer peripheral |
CRC | Cyclic Redundancy Check |
DC fault | (IEC/UL) Short circuits between signals. |
DCC | C2000 dual clock comparitors |
DCSM | C2000 dual code-security module |
ECC | Error correction code |
E/E/PE | (IEC/UL) Electrical/Electronic/Programmable Electronic |
EMC | (IEC/UL) Electromagnetic compatibility |
ePIE | C2000 enhanced peripheral interrupt expansion block. May also be referred to as PIE. |
ePWM | C2000 enhanced Pulse Width Modulation peripheral. May also be referred to as PWM. |
FPU | Floating-point Unit instruction set extension to the C28x CPU |
FSM |
|
GPIO | C2000 general purpose input/output pin |
H.x... | Reference from the IEC 60730 standard. For example: H.2.16.5 is a specific definition found in annex H of the standard. |
HRPWM | High-resolution feature of the C2000 ePWM module |
HW | Hardware (the microcontroller) |
HWBIST | C2000 hardware built-in self test |
IEC | International Electrotechnical Commission |
IEC 60730 | The terms "IEC 60730", "UL 1998", "IEC / UL standards", "60730" and
"the standards" are used interchangeably to refer to both:
|
IEC 61508 | IEC 61508 Functional Safety of Electrical/Electronic/Programmable Electronic Safety-Related Systems, International Electrotechnical Commission, Edition 2.0 2010. |
ISO 26262 | ISO 26262–Road Vehicles-Functional Safety, International Standard ISO, vol. 26262, 2018. |
IEC / UL | Short for the standards or indicates something taken from the standards. Such as (IEC/UL) marked definitions in this list. See IEC 60730 |
MPOST | Memory power-on self-test |
PIE | See ePIE. |
PWM | See ePWM. |
PEST | Periodic self-test |
POST | Power-on self-test |
ROM | Read only memory |
SDL | Software Diagnostic Library |
SRAM | Static random-access memory |
STL | Self-Test Library |
Stuck-at | (IEC/UL) An open circuit fault or non-varying signal level |
SW | Software |
TI | Texas Instruments Inc. |
TMU | Trigonometric Math Unit instruction set extension to the C28x CPU |
UL | Underwriters Laboratories Inc. |
UL 1998 | See IEC 60730 |
Unique ID | A C2000 unique identifier assigned to a functional safety feature or diagnostic in the functional safety manual. For example CLK2 or GPIO4. |
VCRC | Refer to VCU |
VCU | Instruction set extension to the C28x CPU. Part of the added instructions are CRC calculation specific. The CRC instructions are supported on some devices as simply the "VCRC". |