SPRUIF3B May 2017 – March 2019 DRA790 , DRA791 , DRA793 , DRA797
A 2Gb NAND flash memory (x16) is supported as a nonvolatile memory option on the EVM. The device is supported on CS0, and therefore can also be used as a boot device. Booting from the NAND flash memory is supported on the EVM. The onboard MUX must be able to enable the memory by setting SW8.p1 to on. Ensure the correct SoC boot mode is set using the SYS_BOOT switches (SW3 and SW4).