SPRUIF3B May 2017 – March 2019 DRA790 , DRA791 , DRA793 , DRA797
As a primary nonvolatile boot device, the EVM includes 256Mb of Quad-SPI flash memory. The device is supported on CS0 of the QSPI interface. The interface can be configured to support either serial mode (1×) or quad mode (4×).
Booting from the QSPI flash memory is supported on the EVM. No EVM configuration is required because the QSPI flash is enabled by default. Ensure the correct SoC boot mode is set using the SYS_BOOT switches (SW3 and SW4).