SPRUIF3B May 2017 – March 2019 DRA790 , DRA791 , DRA793 , DRA797
Figure 20 is part of the SoC pinmux table for SPI2. The SoC device supports additional functions not shown in the table. The functions shown are intended to reflect those supported on the EVM. These functions include:
Figure 20. SoC Pinmux for SPI2 and UART3 MUX K: Selects between Bluetooth (COM8Q module) and expansion interface. The selection is made using the I/O expander 2, bits P16, defaulting to expansion. Figure 21 shows the MUX diagram for SPI2 and UART3.
Figure 21. MUX Diagram for SPI2 and UART3