SPRUJH3 April 2025 TMS320F2800132 , TMS320F2800133 , TMS320F2800135 , TMS320F2800137 , TMS320F2800152-Q1 , TMS320F2800153-Q1 , TMS320F2800154-Q1 , TMS320F2800155 , TMS320F2800155-Q1 , TMS320F2800156-Q1 , TMS320F2800157 , TMS320F2800157-Q1 , TMS320F280021 , TMS320F280023 , TMS320F280023C , TMS320F280025 , TMS320F280025C , TMS320F280034 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037C , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039C , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041C , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049C , TMS320F28076 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377S , TMS320F28378D , TMS320F28378S , TMS320F28379D , TMS320F28379S , TMS320F28384D , TMS320F28384S , TMS320F28386D , TMS320F28386S , TMS320F28388D , TMS320F28388S , TMS320F28P550SG , TMS320F28P550SJ , TMS320F28P559SG-Q1 , TMS320F28P559SJ-Q1 , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
Before attempting to program the device, understand how the non-volatile memory of C2000 devices works. The Flash memory on C2000 devices allow users to easily erase and re-program the device without losing data after loss of power. Erase operation set all bits in a given sector to 1, while programming operations selectively clear bits to 0.
During development, an application executable can be programmed into the Flash memory using Code Composer Studio™ (CCS) [1]. When CCS identifies that the application code is mapped into the Flash memory, the On-Chip Flash Plugin is automatically invoked to load the executable to the Flash. By default, the plugin erases the Flash before programming, generates the ECC for the executable, and then programs and verifies the application into the Flash.
The Flash Plugin GUI can be used when connected to the target CPU core and found in CCS at:


TI also offers application flashing with UniFlash [2], a standalone JTAG based Flash programming tool with a smaller footprint than that of CCS due to less debug support. Nonetheless, UniFlash provides all the GUI operations that the CCS On-Chip Flash plugin does.