SPRUJH3 April   2025 F28377D-SEP , TMS320F2800132 , TMS320F2800133 , TMS320F2800135 , TMS320F2800137 , TMS320F2800152-Q1 , TMS320F2800153-Q1 , TMS320F2800154-Q1 , TMS320F2800155 , TMS320F2800155-Q1 , TMS320F2800156-Q1 , TMS320F2800157 , TMS320F2800157-Q1 , TMS320F280021 , TMS320F280023 , TMS320F280023C , TMS320F280025 , TMS320F280025C , TMS320F280034 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037C , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039C , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041C , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049C , TMS320F28076 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377S , TMS320F28378D , TMS320F28378S , TMS320F28379D , TMS320F28379S , TMS320F28384D , TMS320F28384S , TMS320F28386D , TMS320F28386S , TMS320F28388D , TMS320F28388S , TMS320F28P550SG , TMS320F28P550SJ , TMS320F28P559SG-Q1 , TMS320F28P559SJ-Q1 , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Configuring the Boot Mode
    1. 2.1 Standalone Boot
      1. 2.1.1 Boot Mode Select Pins (BMSP)
      2. 2.1.2 Boot Definition Table (BOOTDEF)
      3. 2.1.3 Boot ROM OTP Configuration Registers
      4. 2.1.4 CPU2 Boot Flow
    2. 2.2 Emulation Boot
  6. 3Programming the Flash
    1. 3.1 Flash API
    2. 3.2 Flash Kernels
  7. 4Bootloading Code to Flash
    1. 4.1 C2000 Hex Utility
    2. 4.2 Common Boot Modes
      1. 4.2.1 Boot to Flash
      2. 4.2.2 SCI Boot
      3. 4.2.3 CAN Boot
      4. 4.2.4 CAN-FD Boot
      5. 4.2.5 USB Boot
  8. 5FAQ
    1. 5.1 Selecting the BMSP GPIOs with a Software-based Implementation
    2. 5.2 Running a Flash Kernel from the Flash Instead of the RAM
    3. 5.3 No Symbols Defined When Debugging Boot ROM
    4. 5.4 Writing Values in the OTP Using the On-Chip Flash Tool
    5. 5.5 Writing Values in the OTP Using the Flash API Plugin
  9. 6Summary
  10. 7References

Configuring the Boot Mode

At the end of the ROM boot sequence, the device decides if emulation or standalone boot needs to be entered depending on if there is a JTAG debugger connected. This is achieved by reading the "DCON" bit in the JTAG state machine (except for on F2837xD/F2837xS/F2807x devices, which poll the “TRSTn” pin). Emulation boot mimics the standalone boot flow by sourcing registers located in the RAM that are identical in structure and configuration to the boot registers in the One-Time Programmable (OTP) memory. Consequently, emulation boot allows for the boot registers to be written to as many times as necessary.

Note: TI highly recommends using emulation mode to debug and verify correctness of the device boot configurations before attempting to program the OTP, as you can only program the OTP once.

This chapter details the configuration and usage of standalone boot (in Section 2.1) and emulation boot (in Section 2.2), but note that the emulation boot flow is demonstrated later in Section 4.2.