SWRU543B January 2019 – June 2025 CC3230S , CC3230SF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
The I2S format is used in audio interfaces. I2S format is realized by configuring the internal TDM transfer mode to two slots per frame.
I2S format is designed to transfer a stereo channel (left and right) over one data pin. Slots are also commonly referred to as channels. The frame width duration in the I2S format is the same as the slot size. The frame signal is also referred to as word select in the I2S format.
Figure 12-1 shows the I2S protocol.
Figure 12-1 I2S ProtocolFigure 12-2 is a functional diagram of the I2S module.
Figure 12-2 I2S Module