SWRU543B January 2019 – June 2025 CC3230S , CC3230SF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
Disables and unregisters ADC interrupt handler for a specified channel.
Parameters:
This function disables and unregisters ADC interrupt handler for a specified channel. This function also masks off the interrupt in the interrupt controller, so that the interrupt handler is no longer called.
The
ulChannel
parameter should be one of the following:
Returns: