TIDUE53J March   2018  – February 2025 TMS320F28P550SG , TMS320F28P550SJ , TMS320F28P559SG-Q1 , TMS320F28P559SJ-Q1

 

  1.   1
  2.   Description
  3.   Resources
  4.   Features
  5.   Applications
  6.   6
  7. 1System Description
    1. 1.1 Key System Specifications
  8. 2System Overview
    1. 2.1 Block Diagram
    2. 2.2 Highlighted Products
      1. 2.2.1  UCC21710
      2. 2.2.2  UCC5350
      3. 2.2.3  TMS320F28379D
      4. 2.2.4  AMC3306M05
      5. 2.2.5  OPA4388
      6. 2.2.6  TMCS1123
      7. 2.2.7  AMC0330R
      8. 2.2.8  AMC0381D
      9. 2.2.9  UCC14341
      10. 2.2.10 UCC33421
    3. 2.3 System Design Theory
      1. 2.3.1 Three-Phase T-Type Inverter
        1. 2.3.1.1 Architecture Overview
        2. 2.3.1.2 LCL Filter Design
        3. 2.3.1.3 Inductor Design
        4. 2.3.1.4 SiC MOSFETs Selection
        5. 2.3.1.5 Loss Estimations
      2. 2.3.2 Voltage Sensing
      3. 2.3.3 Current Sensing
      4. 2.3.4 System Auxiliary Power Supply
      5. 2.3.5 Gate Drivers
        1. 2.3.5.1 1200-V SiC MOSFETs
        2. 2.3.5.2 650-V SiC MOSFETs
        3. 2.3.5.3 Gate Driver Bias Supply
      6. 2.3.6 Control Design
        1. 2.3.6.1 Current Loop Design
        2. 2.3.6.2 PFC DC Bus Voltage Regulation Loop Design
  9. 3Hardware, Software, Testing Requirements, and Test Results
    1. 3.1 Required Hardware and Software
      1. 3.1.1 Hardware
        1. 3.1.1.1 Test Hardware Required
        2. 3.1.1.2 Microcontroller Resources Used on the Design (TMS320F28379D)
        3. 3.1.1.3 F28377D, F28379D Control-Card Settings
        4. 3.1.1.4 Microcontroller Resources Used on the Design (TMS320F280039C)
      2. 3.1.2 Software
        1. 3.1.2.1 Getting Started With Firmware
          1. 3.1.2.1.1 Opening the CCS project
          2. 3.1.2.1.2 Digital Power SDK Software Architecture
          3. 3.1.2.1.3 Interrupts and Lab Structure
          4. 3.1.2.1.4 Building, Loading, and Debugging the Firmware
          5. 3.1.2.1.5 CPU Loading
        2. 3.1.2.2 Protection Scheme
        3. 3.1.2.3 PWM Switching Scheme
        4. 3.1.2.4 ADC Loading
    2. 3.2 Testing and Results
      1. 3.2.1 Lab 1
      2. 3.2.2 Testing Inverter Operation
        1. 3.2.2.1 Lab 2
        2. 3.2.2.2 Lab 3
        3. 3.2.2.3 Lab 4
      3. 3.2.3 Testing PFC Operation
        1. 3.2.3.1 Lab 5
        2. 3.2.3.2 Lab 6
        3. 3.2.3.3 Lab 7
      4. 3.2.4 Test Setup for Efficiency
      5. 3.2.5 Test Results
        1. 3.2.5.1 PFC Mode
          1. 3.2.5.1.1 PFC Start-Up – 230 VRMS, 400 VL-L AC Voltage
          2. 3.2.5.1.2 Steady State Results - PFC Mode
          3. 3.2.5.1.3 Efficiency, THD, and Power Factor Results, 60 Hz – PFC Mode
          4. 3.2.5.1.4 Transient Test With Step Load Change
        2. 3.2.5.2 Inverter Mode
  10. 4Design Files
    1. 4.1 Schematics
    2. 4.2 Bill of Materials
    3. 4.3 PCB Layout Recommendations
      1. 4.3.1 Layout Prints
    4. 4.4 Altium Project
    5. 4.5 Gerber Files
    6. 4.6 Assembly Drawings
  11. 5Trademarks
  12. 6About the Authors
  13. 7Revision History

Architecture Overview

To understand the impetus behind a three level t-type inverter, some background on a traditional two-level inverter is required. Figure 2-4 shows a typical implementation of this architecture.

TIDA-01606 Two-Level, Three-Phase Inverter ArchitectureFigure 2-4 Two-Level, Three-Phase Inverter Architecture

To simplify the analysis, a single leg can be isolated.

TIDA-01606 Two-Level, Single-Phase Inverter LegFigure 2-5 Two-Level, Single-Phase Inverter Leg

In this example, the two switching devices as a pair have four possible conduction states, independent of the other phases.

TIDA-01606 Q1 and Q2 offFigure 2-6 Q1 and Q2 off
TIDA-01606 Q1 off, and Q2 onFigure 2-8 Q1 off, and Q2 on
TIDA-01606 Q1 on, and Q2 offFigure 2-7 Q1 on, and Q2 off
TIDA-01606 Q1 and Q2 on (Invalid)Figure 2-9 Q1 and Q2 on (Invalid)

By observing the current path through the inverter, each switching device must be capable of blocking the full DC link voltage present between DC+ and DC–. In traditional low-voltage systems (< 600 V), this capability is fairly trivial with common off-the-shelf IGBTs. However, if the DC link voltage is pushed higher to increase the power throughput without increasing current, as is a common trend in power electronics, this limitation puts an upper level on the supported voltage ranges.

Additionally, the increased voltage does result in increased switching losses in the traditional IGBTs. The low dV/dt exacerbates in these devices, even when able to support the higher voltages. This dV/dt is what determines how quickly one device can transition from on to off (or vice versa), thus dictating the dead time between each of these states. An elongated switch time or dead time means the switches spend less time at full conduction, resulting in decreased efficiency.

These two primary drawbacks of a two-level inverter are what drives the implementation in this design.

The next step up from a standard two-level inverter is a T-type three-level inverter. This type is implemented by inserting two back-to-back switching devices between the switch node and the neutral point of the DC link created by the bulk input capacitors. These two switch devices are placed in a common emitter configuration so that current flow can be controlled by switching one or the other on or off. This configuration also enables both of them to share a common bias supply as the gate-emitter voltage is identically referenced. Figure 2-10 shows a simplified view of the implementation.

Note:

The E6 hardware middle switches are configured as common source switches. However, the E7 hardware middle switches are configured as common drain switches. The following T-type example illustrations are done using common source configuration.

TIDA-01606 Three-Level T-Type, Three-Phase Inverter ArchitectureFigure 2-10 Three-Level T-Type, Three-Phase Inverter Architecture

To assist in understanding the benefits of the architecture, the inverter is again reduced to a single leg.

TIDA-01606 Three-Level T-Type, Single-Phase Inverter LegFigure 2-11 Three-Level T-Type, Single-Phase Inverter Leg

Adding two extra switching devices complicates the control of the system, but the same process of evaluating current flow during various modulation points illustrates the architecture benefits. Additionally, a simplified commutation scheme can be demonstrated, illustrating that control of a T-type inverter is not substantially more difficult than a traditional two-level architecture.

A single leg has three potential connection states: DC+, DC–, or N. This connection can be accomplished by closing Q1, closing Q3 and Q4, and closing Q2, respectively. However, this scheme depends on the current path in the system. Rather, for a DC+ connection, Q1 and Q3 can be closed, Q2 and Q4 for a neutral connection, and Q2 and Q4 for a DC– connection. This scheme acts independent of current direction as shown in the following figures.

TIDA-01606 Q1 on, Q2 off, Q3 on, and Q4 offFigure 2-12 Q1 on, Q2 off, Q3 on, and Q4 off
TIDA-01606 Q1 off, Q2 off, Q3 on, and Q4 onFigure 2-14 Q1 off, Q2 off, Q3 on, and Q4 on
TIDA-01606 Q1 off, Q2 off, Q3 on, and Q4 offFigure 2-13 Q1 off, Q2 off, Q3 on, and Q4 off

This example starts with the output phase connected to DC+ by closing Q1 and Q3, resulting in current output from the system. To transition to an N connection, Q1 is opened and after a dead-time delay, and Q4 is closed. This setup allows current to naturally flow through Q3 and the diode of Q4.

TIDA-01606 Q1 on, Q2 off, Q3 on, and Q4 offFigure 2-15 Q1 on, Q2 off, Q3 on, and Q4 off
TIDA-01606 Q1 off, Q2 off, Q3 on, and Q4 onFigure 2-17 Q1 off, Q2 off, Q3 on, and Q4 on
TIDA-01606 Q1 off, Q2 off, Q3 on, and Q4 offFigure 2-16 Q1 off, Q2 off, Q3 on, and Q4 off

For a negative current, the same sequence can be used. Once Q4 is closed, current then flows through Q4 and the diode of Q3 rather than the diode of Q1.

TIDA-01606 Q1 off, Q2 off, Q3 on, Q4 onFigure 2-18 Q1 off, Q2 off, Q3 on, Q4 on
TIDA-01606 Q1 on, Q2 off, Q3 on, Q4 offFigure 2-20 Q1 on, Q2 off, Q3 on, Q4 off
TIDA-01606 Q1 off, Q2 off, Q3 on, Q4 offFigure 2-19 Q1 off, Q2 off, Q3 on, Q4 off

A similar natural current flow can be observed when connecting the output leg from N to DC+ with a positive current. Q3 and Q4 start closed with a full N connection. Q4 is switched off, but current still flows through the associated diode. Closing Q1 now naturally switches the current flow from N to DC+.

TIDA-01606 Q1 off, Q2 off, Q3 on, Q4 onFigure 2-21 Q1 off, Q2 off, Q3 on, Q4 on
TIDA-01606 Q1 on, Q2 off, Q3 on, Q4 offFigure 2-23 Q1 on, Q2 off, Q3 on, Q4 off
TIDA-01606 Q1 off, Q2 off, Q3 on, Q4 offFigure 2-22 Q1 off, Q2 off, Q3 on, Q4 off

As in the earlier example when moving from a DC+ to N connection on a negative current, the same scheme can also be used here for a positive current. Q3 and Q4 begin closed, conducting current into N. Q4 is opened, causing current to flow through the diode of Q1. Lastly, Q1 is closed, and current continues flowing in the same direction.

All four of these transition states (DC+ to N, N to DC+, with both forward and reverse current) all share two simple switching schemes. This also holds true for transitions to and from DC– through Q2. By maintaining this scheme through all switching cycles, a simple dead-zone delay between switching events is all that is needed to avoid shoot-though; however, additional protection can be added in the control software with relative ease.

An additional benefit from this modulation scheme is that Q3 and Q4 never switch at the same time. This benefit reduces voltage stress on the devices as well as the power rating of the bias supply to drive these devices effectively. As previously mentioned, Q3 and Q4 can share a single supply sized for one driver rather than two.

Q1 and Q2 still need to block the full DC link voltage as the inverters do in the traditional architecture. To use a higher DC bus voltage, full-voltage FETs must still be in place; however, because the inverters are back to back and do not switch at the same time, the two switches on the center leg can be at a lower rating.