Motor Drive and Control

For various motor types; AC Induction (ACIM), Brushed DC , Brushless DC (BLDC), Permanent Magnet Synchronous and Stepper find the right analog and digital products, software and support to precisely control the position, velocity and torque

New TI Motor Solutions Guide

New TI Motor
Solutions Guide

TI Spins Motors into a new 16 page solution guide, with answers to your toughest motor questions.

Industrial Automation - Motor Control Solutions Guide

Industrial Automation Solutions Guide

TI's Motor Drive and Control solutions speed the design cycle with the right devices, software, tools and support.

InstaSPIN Inside - BLDC Motors - Motor Control Solutions

TI's InstaSPIN™-BLDC Solution

Unlike traditional back-emf zero crossing techniques, InstaSPIN-BLDC extends sensorless operation down to lower speeds, and exhibits high immunity to miscommutation caused by rapid speed changes.


 

InstaSPIN™-BLDC Solution

In keeping with TI’s philosophy of making motor control more accessible and easier to use by design engineers, TI is proud to announce the release of its newest motor control technology, InstaSPIN-BLDC.  Targeted at low cost BLDC applications, InstaSPIN-BLDC is a sensorless control technique based on the premise that “simple is better”. In field tests with over 50 different motor types, InstaSPIN-BLDC was able to get each motor up and running in less than 20 seconds!  The reason for this incredible robustness is because InstaSPIN-BLDC doesn’t require any knowledge about motor parameters to work, and you only need to adjust a single tuning value.

Unlike other sensorless BLDC control techniques based on back-EMF zero-cross timing, InstaSPIN-BLDC monitors the motor’s flux to determine when to commutate the motor. With the help of a free GUI (see figure), the user can watch the flux signal in a plot window, and set the “Flux Threshold” slider to specify at what flux level the motor should be commutated.  Optimal commutation can be verified by observing the phase voltage and current waveforms, which are also displayed.

In addition to its ability to work with just about ANY BLDC motor, InstaSPIN-BLDC has demonstrated incredible resilience to speed transient perturbations.  With zero-cross timing, you are always using PAST information to predict FUTURE commutation events.  But InstaSPIN-BLDC monitors a real-time flux waveform to determine the appropriate time to commutate.  Abrupt speed changes will be reflected in the flux waveform in real time, so that it will still cross the specified threshold value at exactly the right time to commutate.

Using flux for commutation vs. back-EMF zero-cross timing also enables more stable operation at lower speeds.  Unlike the flux signal, the back-EMF signal amplitude diminishes at lower speeds, resulting in poor signal-to-noise performance.  InstaSPIN-BLDC enables smoother operation at low speeds, and provides more reliable motor starting, even under heavy loads.

Get InstaSPIN™-BLDC

Piccolo family of microcontrollers

Stellaris ARM®Cortex™-M based MCUs

MSP430™16-bit Ultra-Low Power MCUs

  • Coming 1Q12

InstaSPIN-BLDC Software Solution


Videos

video platform video management video solutions video player {SEO}