SPRADJ0 February   2025 AM2612 , AM2631 , AM2632 , AM2634 , AM263P2 , AM263P4 , AM2732 , AM2732-Q1 , AM620-Q1 , AM623 , AM625 , AM625-Q1 , AM62A3 , AM62A3-Q1 , AM62A7 , AM62A7-Q1 , AM62D-Q1 , AM62P , AM62P-Q1 , AM67 , AM68A , AM69A , DRA821U , TDA4AEN-Q1 , TDA4AH-Q1 , TDA4AL-Q1 , TDA4AP-Q1 , TDA4VE-Q1 , TDA4VEN-Q1 , TDA4VH-Q1 , TDA4VL-Q1 , TDA4VM , TDA4VP-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
    1. 1.1 Configurator
  5. 2Software Stack
    1. 2.1 Configurator Plug-in
    2. 2.2 Source Files
    3. 2.3 User Guide
    4. 2.4 Compliance Support Package (CSP)
  6. 3Utilizing the Source - Building Drivers and Examples
    1. 3.1 One-Time Setup
    2. 3.2 Build Instructions
    3. 3.3 Build Command Syntax
  7. 4Obtaining an MCAL package
  8. 5Summary
  9. 6References

Obtaining an MCAL package

Texas Instruments delivers MCAL packages for utilization on devices as both: AUTOSAR stack bundle from several of the top entire stack vendors such as Vector, ETAS, and as a standalone MCAL+CDD bundle which can be requested from your nearest customer support and field engineer who can share TI's license export form on the latest MCAL version in TI's official website. Examples include: MCAL AM263x v10.00.00, MCAL AM263Px v10.00.00, and MCAL AM273x v09.01.00. Similarly for Sitara MPU devices and the Jacinto 7 entry device, the MCAL+CDD standalone bundle can be requested from the nearest customer support or field engineers or through the Software Export request form. Examples include: MCAL AM62x v10.00.00, MCU+SDK AM62x v10.00.00, and Processor SDK RTOS (MCU+ SDK) J722S v10.00.00. The MCAL versions are matched with device MCU+SDK release versions. MCAL for the remaining Jacinto devices is publicly available on TI's website ti.com under the MCUSW folder as part of RTOS SDK (example: J721E RTOS SDK), where the configurator plug-ins package for the drivers must be requested separately.

While requesting an MCAL package, the EB tresos Studio User License can also be requested to make use of the configurator plug-ins in TI's partner Configurator tool.

MCAL started on AM263x and AM273x Sitara MCUs with the v08.06 release at the beginning of 2023, followed by several releases. The latest release of v09.02.00 was in May 2024. MCALs have previously been available for Sitara MPU and Jacinto family of devices, the latest version is v10.00. These release versions also follow semantic versioning as explained under the introduction section for earlier AUTOSAR standard versions and according to the device SDK (MCU-PLUS-SDK) release version of the timeline available for a device from TI's official website.

Many other releases and long-term support are planned for MCALs available for various products, including the MCAL packages for Jacinto, Sitara MPU, Sitara MCU, C2000, Hercules MCU, Radar, MSP, and any other such TI devices.