SBASAE3 December 2025 ADS125H18
PRODUCTION DATA
Another method to determine when data are ready is to count ADC main clock cycles. This method is only possible when using an external clock because the internal clock oscillator is not observable. After synchronization or conversion start, the number of clock cycles is larger compared to the normal conversion data period. The initial number of clock cycles is equal to the latency time of the digital filter as listed in the Digital Filter section.