SLVSIF4 September 2026 TPS481HS04-Q1
ADVANCE INFORMATION
The CONFIG/ACTIVE state is where the device stays during normal operation when the outputs are OFF (CONFIG) or ON (ACTIVE). The difference between the two is that in the CONFIG state (with the outputs OFF) all of the registers can be configured. The configuration registers (especially ones needed for to successfully enable the channel) are expected to be written to before the outputs can be turned ON, when transitioning from the SLEEP mode (and all the registers are lost). However, the configuration registers are retained while in the LPM and so the device does not need to be reconfigured while tranisitioning from the LPM to the ACTIVE state. The quiescent current draw from VBB, (IQVBB) and VDD, (IQVVD) is higher than in the other states to support the load and device diagnostics. SPI communication and diagnostics checks are fully supported in this state.