SLVSIF4 September 2026 TPS481HS04-Q1
ADVANCE INFORMATION
The TPS481HS04-Q1 provides an integrated successive approximation 10-bit ADC which can convert different analog signals to digital signals which can be read out through SPI. The ADC can convert the following analog signals:
Figure 7-8 provides a functional block diagram of the integrated ADC along with the analog signal inputs to the ADC.
Conversion of any of the analog signals can either be disabled globally through the ADC_CONFIG register.
The device also provides a configurable delay which can also help to further reduce the quiescent current of the device by reducing the sampling rate of the ADC. The configurable delay is set by the ADC_CONFIG_DELAY [1:0] bits in the ADC_CONFIG register.
If I2T protection is enabled (I2T_EN_CHx = 1) and either channel is not in I2T mode (I2T_MOD_CHx = 0), then the device will convert each of the analog signals in a round robin sequence with the configurable delay. Figure below shows the ADC scheduling if no channel is in I2T mode (I2T_MOD_CHx = 0) and all analog signal conversions are enabled. If I2T protection is disabled then the round robin sequence below also applies.
If I2T protection is enabled (I2T_EN_CHx = 1) and one or both of the channels are in I2T mode (I2T_MOD_CHx = 1), then the device disables all conversions except for the ISNSx conversions which are used for the internal I2T protection. The device also disables the configurable delay function as well. Figure below shows the ADC scheduling if one or both of the channels are in I2T mode (I2T_MOD_CHx = 1).