SLVSIF4 September 2026 TPS481HS04-Q1
ADVANCE INFORMATION
The device includes a temperature sensor on the power FET and within the controller portion of the device to monitor the temperature of the FET (TJ,FET) and the temperature of the controller (TJ,CONTROLLER). There are two cases that the device will consider to be a thermal shutdown fault:
If either of the above faults occur, the switch will be turned off. The device will signal a fault through the FLT/WAKE pin.
A relative thermal shutdown event can occur when there is a large peak power event such as a short-to-ground event where the FET temperature (TJ,FET) quickly rises relative to the controller temperature (TJ,CONTROLLER). Once the relative temperature (TJ,FET – TJ,CONTROLLER) exceeds TREL the channel will be turned off.
An absolute thermal shutdown occurs when the FET temperature (TJ,FET) rises above TABS. This can occur when a channel is subjected to long durations of overcurrent such as a permanent short use case. Once the FET temperature (TJ,FET) exceeds TABS the channel will be turned off.