SPRACP3D November 2019 – August 2026 AWR6843 , AWR6843AOP , IWR1443 , IWR1642 , IWR6443 , IWR6843 , IWR6843AOP
Problem statement: Device is not transmitting within the permitted ISM occupied bandwidth.
Solution: Update signal bandwidth as needed.
Deep Dive:
According to Draft ETSI EN 305 550V2.1.0, occupied bandwidth is defined as the width of a frequency band such that, below the lower and above the upper frequency limits, the mean powers emitted are each equal to 0.5% of the total mean power of a given emission. This roughly corresponds to the –23dBc bandwidth of the signal.
For larger bandwidth, such as the 4GHz bandwidth, there is a large frequency jump from (64GHz to 60GHz) which results in undershoots, affects the settling time, and can result in failure of the –23dBc bandwidth limit.
For example, the 1300MHz use case in the bandwidth is determine as shown in Table 6-1: it can be changed by either changing the slope or chirp parameter in the chirp config.
| Bandwidth | ProfileCFG |
|---|---|
| 1300MHz | ar1.ProfileConfig(0, 60.25, 3.6, 3.5, 29.7,0, 0, 0, 0, 0, 0, 43.995, 1, 256, 10000, 0, 131072, 30) |