SPRACP3D November 2019 – August 2026 AWR6843 , AWR6843AOP , IWR1443 , IWR1642 , IWR6443 , IWR6843 , IWR6843AOP
The following criteria applies for the test per the standard for EMC emissions and immunity.
| Criterion | During Test | After Test |
|---|---|---|
| A | Operate as intended. No loss of function. No unintentional responses | Operate as intended. No loss of function. No degradation of performance. No loss of stored data or user programmable functions. |
| B | Can show loss of function. No unintentional responses | Operate as intended. Lost functions shall be self-recoverable. No degradation of performance. No loss of stored data or user programmable functions. |
The following clauses under EN 301 489-1 are applicable to the TI IWR6843 and MMWAVEICBOOST Evaluation Board combo. Since the equipment requires DC power and is not a telecommunication equipment, some of the tests do not apply. Users must determine which test is applicable to their end equipment.
| Environmental phenomenon | Verdict | |
|---|---|---|
| Enclosure of ancillary equipment measured on a standalone basis – Clause 8.2 | Ancillary equipment Class B limits given in EN 55032 | Pass |
| Ancillary equipment Radiated disturbance above 1GHz at a measurement distance of 3m | Pass | |
| Ancillary equipment intended to be used in telecommunication centers only Class A limits given in EN 55032 | Not applicable | |
| Ancillary equipment intended to be used in telecommunication centers only Radiated disturbance above 1GHz at a measurement distance of 3m | Not applicable | |
| DC power input/output ports – Clause 8.3 | Class B limits according to EN 55032 | Pass |
| Equipment intended to be used in telecommunication centers only | Not applicable | |
| AC mains power input/output ports – Clause 8.4 | Class B limits given in EN 55032 | Not applicable |
| Equipment intended to be used in telecommunication centers only Class A limits given in EN 55032 | Not applicable | |
| Harmonic current emissions (AC mains input port)– Clause 8.5 | The appropriate requirements of EN 61000-3-2/A1 for harmonic current emission apply for equipment with an input current up to and including 16A per phase. For equipment with an input current of greater than 16A per phase EN 61000-3-12 applies. | Not applicable |
| Voltage fluctuations and flicker (AC mains input port) – Clause 8.6 | The appropriate requirements of EN 61000-3-3 for voltage fluctuations and flicker apply for equipment with an input current up to and including 16A per phase. For equipment with an input current of greater than 16A per phase EN 61000-3-11 [13] applies. | Not applicable |
| Telecommunication ports – Clause 8.7 | Class B limits given in EN 55032 | Not applicable |
| Equipment intended to be used in telecommunication centers only Class A limits given in EN 55032 | Not applicable | |
| Environmental phenomenon | Test port | Basic standard | Verdict |
|---|---|---|---|
| Radio frequency electromagnetic field (80MHz to 1000MHz and 1000MHz to 6000MHz) – Clause 9.2 | Enclosure | EN 61000-4-3 | Pass |
| Electrostatic discharge1 – Clause 9.3 | Enclosure | EN 61000-4-2 | Pass |
| Fast transients, Common mode– Clause 9.4 | AC mains power port | EN 61000-4-4 | Not applicable |
| Signal ports, telecommunication ports, control ports | Not applicable | ||
| DC power ports | Pass | ||
| Radio frequency, common mode (0.15MHz to 80MHz) – Clause 9.5 | AC mains power port | EN 61000-4-6 | Not applicable |
| Signal ports, telecommunication ports, control ports | Not applicable | ||
| DC power ports | Pass | ||
| Transients and surges – Clause 9.6 | 12V and 24V DC supply voltage input ports of mobile radio and ancillary equipment, which are also intended for mobile use in vehicles. | ISO 7637-2 | Not applicable |
| Voltage dips and interruptions – Clause 9.7 | AC mains power port | EN 61000-4-11 | Not applicable |
| Surges line to line and line to ground – Clause 9.8 | AC mains power port | EN 61000-4-5 | Not applicable |
| Telecommunication ports | Not applicable | ||
In addition to EN 301 489-1, there are standards which apply EN 301 489-1 to specific end equipments. They are explanatory and provide more granular detail on how to apply the standards contained within EN 301 489-1. For most 60GHz radars, EN 301 489-3 will be used. It provides clarifications for how EN 301 489-1 should be interpreted. Four key provisions apply here.
The first is that the device must be tested with transmit signals representative of actual use and receive signals for radiated immunity must be 30dB higher than the minimum usable signal. Provisions are made for the case where the defined signal causes saturation of the receiver.
The second, is the recognition of different modes of operation, such as "power off", "standby", and so forth. These modes are typically determined through a reading of the theory of operation. The device should not have an unplanned transmission during its non transmit mode.
The third, is the introduction of clarity of when radiated and conducted emissions at specific ports are applicable. This is covered in Table 4 of EN 301 489-3. From Table 4, radiated emissions are generally applicable to all equipment, DC power input/output port conducted emissions are required for all non-portable use equipment and finally AC mains input/output and wired network conduced emissions only applies to fixed location equipment.
Ultimately EN 301 489-3 shouldn't add any additional testing; rather EN 301 489-3 simply makes clear the requirements of EN 301 489-1 as applied to radars and other specific SRD niches.