SPRACP3D November 2019 – August 2026 AWR6843 , AWR6843AOP , IWR1443 , IWR1642 , IWR6443 , IWR6843 , IWR6843AOP
EIRP is defined as the sum of the transmitted power and antenna gain, when these two parameters are known the EIRP can be calculated as in Equation 9. EIRP indicates the maximum radiated power at the peak angle of a non-isotropic antenna.
where