- The shield or absorber must be placed as shown in Figure 6-3 and Figure 6-4.
- Applicable mmWave devices, decoupling caps, crystal, and the surrounding PCB
area must be covered by a shield or absorber.
- The shield must be well grounded, covering the components of interest, and
absorbers must be properly adhered to PCB and components of interest.
- Make sure the height of the shield from the PCB is greater than or equal to 2mm
above the RF traces; otherwise the RF transmission lines can couple with the shield and RF
matching can get disturbed. Manufacturing tolerances, wear and tear, shield assembly, and
so forth must be considered so that a 2mm+ height from the board is always
maintained.
- When using an RF absorber, the antenna must not be covered; the absorber must
be placed such that the absorber does not go beyond the edge of the IC on the areas with
the TX and RX traces.
- Example of an absorber used to suppress the emission is Cuming Microwave (GDX/PPGA 0.03").