SPRADM0 August   2025 F28E120SC , F29H850TU , F29H859TU-Q1 , TMS320F2800132 , TMS320F2800133 , TMS320F2800135 , TMS320F2800137 , TMS320F2800152-Q1 , TMS320F2800153-Q1 , TMS320F2800154-Q1 , TMS320F2800155 , TMS320F2800155-Q1 , TMS320F2800156-Q1 , TMS320F2800157 , TMS320F2800157-Q1 , TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1 , TMS320F28075 , TMS320F28075-Q1 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377D-EP , TMS320F28377D-Q1 , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S , TMS320F28384D , TMS320F28384S , TMS320F28386D , TMS320F28386S , TMS320F28388D , TMS320F28388S , TMS320F28P550SG , TMS320F28P550SJ , TMS320F28P559SG-Q1 , TMS320F28P559SJ-Q1 , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. Introduction
  5. Hardware Setup Options
    1. 2.1 Setup #1
    2. 2.2 Setup #2
    3. 2.3 Setup #3
    4. 2.4 Setup #4
  6. Software Layers
  7. GUI Creation
  8. Application Logging
    1. 5.1 Application Logging Walk-through
  9. Transfer Bridge
    1. 6.1 Transfer Bridge Walk-through
  10. Communication Logger
    1. 7.1 Communication Logger Walk-through
  11. Rapid-Time Logger
    1. 8.1 Rapid Time Logging Walk-through
  12. Transfer Examples Overview
  13. 10Summary
  14. 11References

Setup #3

The third hardware setup is possible only if the data logging (primary) device has a FSI peripheral present and the bridge device has both an FSI and a USB peripheral present. This setup uses the FSI peripheral on a standalone part to export data out of the device and a bridge device to convert these messages to a USB protocol that the PC can understand. If using a controlCARD for the bridge device, the USB signals are already correctly wired to a USB connector that can be plugged into a PC. Both the FSI code on the primary device and the FSI-to-USB code on the bridge device need to be configured, which can both be done automatically by the MCU Control Center tool in two separate Sysconfig projects. See more details in later sections.

Note that if there is no controlCARD at the user's disposal, but only a standalone part that has the FSI and USB peripheral and can be used as the bridge device, USB connector circuitry is needed to connect to a USB port.

 Hardware Setup #3Figure 2-3 Hardware Setup #3