SPRADM0 August   2025 F28E120SC , F29H850TU , F29H859TU-Q1 , TMS320F2800132 , TMS320F2800133 , TMS320F2800135 , TMS320F2800137 , TMS320F2800152-Q1 , TMS320F2800153-Q1 , TMS320F2800154-Q1 , TMS320F2800155 , TMS320F2800155-Q1 , TMS320F2800156-Q1 , TMS320F2800157 , TMS320F2800157-Q1 , TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1 , TMS320F28075 , TMS320F28075-Q1 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377D-EP , TMS320F28377D-Q1 , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S , TMS320F28384D , TMS320F28384S , TMS320F28386D , TMS320F28386S , TMS320F28388D , TMS320F28388S , TMS320F28P550SG , TMS320F28P550SJ , TMS320F28P559SG-Q1 , TMS320F28P559SJ-Q1 , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. Introduction
  5. Hardware Setup Options
    1. 2.1 Setup #1
    2. 2.2 Setup #2
    3. 2.3 Setup #3
    4. 2.4 Setup #4
  6. Software Layers
  7. GUI Creation
  8. Application Logging
    1. 5.1 Application Logging Walk-through
  9. Transfer Bridge
    1. 6.1 Transfer Bridge Walk-through
  10. Communication Logger
    1. 7.1 Communication Logger Walk-through
  11. Rapid-Time Logger
    1. 8.1 Rapid Time Logging Walk-through
  12. Transfer Examples Overview
  13. 10Summary
  14. 11References

Setup #4

The fourth hardware setup is possible only if both the data logging (primary) device and first bridge device has an FSI peripheral present. This setup uses the FSI peripheral to export data out of a standalone device, one bridge device to convert these messages to a UART protocol, and a second bridge device to convert these messages from a UART protocol to a USB protocol that the PC can understand.

If using a LaunchPAD or controlCARD of a C2000 device with a FSI peripheral, both bridge devices are already present and correctly wired. The second bridge device on the board has also already been flashed with a program that does the necessary protocol conversion between UART and USB (in most cases this is the XDS110 debugger). This leaves the FSI code on the primary device to be configured, as well as the FSI-to-UART bridge code on the first bridge device to be configured. The configurations for both for both of these devices can be done automatically by the MCU Control Center tool (in two separate Sysconfig projects). More detail is provided in later in the document.

 Hardware Setup #4Figure 2-4 Hardware Setup #4