SPRADM0 August   2025 F28377D-SEP , F28E120SC , F29H850DM , F29H850DU , F29H850TU , F29H859TU-Q1 , F29P329SM-Q1 , F29P580DM , F29P589DM-Q1 , F29P589DU-Q1 , TMS320F2800132 , TMS320F2800133 , TMS320F2800135 , TMS320F2800137 , TMS320F2800152-Q1 , TMS320F2800153-Q1 , TMS320F2800154-Q1 , TMS320F2800155 , TMS320F2800155-Q1 , TMS320F2800156-Q1 , TMS320F2800157 , TMS320F2800157-Q1 , TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1 , TMS320F28075 , TMS320F28075-Q1 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377D-EP , TMS320F28377D-Q1 , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S , TMS320F28384D , TMS320F28384S , TMS320F28386D , TMS320F28386S , TMS320F28388D , TMS320F28388S , TMS320F28P550SG , TMS320F28P550SJ , TMS320F28P559SG-Q1 , TMS320F28P559SJ-Q1 , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1 Introduction
  5. 2 Hardware Setup Options
    1. 2.1 Setup #1
    2. 2.2 Setup #2
    3. 2.3 Setup #3
    4. 2.4 Setup #4
  6. 3 Software Layers
  7. 4 GUI Creation
  8. 5 Application Logging
    1. 5.1 Application Logging Walk-through
  9. 6 Transfer Bridge
    1. 6.1 Transfer Bridge Walk-through
  10. 7 Communication Logger
    1. 7.1 Communication Logger Walk-through
  11. 8 Rapid-Time Logger
    1. 8.1 Rapid Time Logging Walk-through
  12. 9 Transfer Examples Overview
  13. 10Summary
  14. 11References

GUI Creation

The GUI layer leverages GUI Composer on the PC and can be run inside the CCS environment. For more information regarding GUI Composer, refer to the GUI Composer Documentation. The following files are generated to create the GUI composer application once the MCU Control Center Sysconfig module is added to the project.

 SysCfg Generated GUI Layer
                    Files Figure 4-1 SysCfg Generated GUI Layer Files

The following post build step is required for generating the custom GUI application for CCS. Navigate to Properties -> General -> Variables for the specific project and add a variable called GUI_SUPPORT.

 Open Project Properties Figure 4-2 Open Project Properties
 Add CCS Variable Figure 4-3 Add CCS Variable
 GUI_SUPPORT Variable Added Figure 4-4 GUI_SUPPORT Variable Added

Additionally, in the project properties, add the following line to the post build step by going to Build → Steps:

if ${GUI_SUPPORT} == 1 ${BuildDirectory}\syscfg\gui_setup.bat

Before building the project, make sure the GUI_SUPPORT variable is set to 1. This copies the GUI files autogenerated by Sysconfig into the proper location in the CCS installation folder at the end of each project build. Once placed in that folder, the GUI application can be successfully launched straight from inside the CCS environment. Once built, the autogenerated GUI project name matches the name selected in the Sysconfig setting below.

 Plugin Name Figure 4-5 Plugin Name

After building the project, refresh the CCS View to see the newly generated GUI in the CCS plugins dropdown. Go to Help → Reload Window.

 Reload Window To See Generated
                    Plugins Figure 4-6 Reload Window To See Generated Plugins

To open the integrated GUI application, go to View → Plugins → {NameOfGUI}. The GUI opens up in CCS once clicked on.

 View GUI Figure 4-7 View GUI