SPRADO2C November 2024 – September 2025 AM62A1-Q1 , AM62A3 , AM62A3-Q1 , AM62A7 , AM62A7-Q1 , AM62D-Q1
During the custom board design cycle, the recommendation is to follow Hardware Design Considerations for Custom Board Design Using AM62A7, AM62A7-Q1, AM62A3, AM62A3- Q1, AM62A1-Q1 and AM62D-Q1 Processor Families user's guide along with Schematic Design Guidelines and Schematic Review Checklist user's guide.
There is no firm rule or requirement for external pull unless the pull requirements are defined in an industry standard. Industry standard definition for pulls is the main reason we can make firm recommendations for external pulls on the eMMC and SD card signals. For the other peripherals, the recommendation is for customers to evaluate the function of the attached devices connected to every processor signal on the custom board and apply the appropriate technical/engineering judgment to determine the need to have external pulls that prevent any input from floating when attached device inputs buffer is turned on. The recommendations provided in the design guide are generic and customer is expected to review the design requirements and the availability of pulls internal to the attached device before implementing. Be sure to not provide an external pull in contention with an internal pull. Example: An example is adding an external pull that is in contention with the internal pull (internal to the attached device), such that the contention creates a mid-supply potential on the signal (input).