SPRUHX5I August 2014 – May 2024 TMS320F28374S , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376S , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28378S , TMS320F28379S
The transmitter interrupt (XINT) signals the CPU of changes to the serial port status. Four options exist for configuring this interrupt. The options are set by the transmit interrupt mode bits, XINTM, in SPCR2.
| Register | Bit | Name | Function | Type | Reset Value | |
|---|---|---|---|---|---|---|
| SPCR2 | 5-4 | XINTM | Transmit interrupt mode | R/W | 00 | |
| XINTM = 00 | XINT generated when XRDY changes from 0 to 1. | |||||
| XINTM = 01 | XINT generated by an end-of-block or end-of-frame condition in a transmit multichannel selection mode. In any of the transmit multichannel selection modes, interrupt after every 16-channel block boundary has been crossed within a frame and at the end of the frame. For details, see Section 20.6.8. In any other serial transfer case, this setting is not applicable and, therefore, no interrupts are generated. | |||||
| XINTM = 10 | XINT generated by a new transmit frame-synchronization pulse. Interrupt on detection of each transmit frame-synchronization pulse. This generates an interrupt even when the transmitter is in the reset state. This is done by synchronizing the incoming frame-synchronization pulse to the CPU clock and sending the pulse to the CPU using XINT. | |||||
| XINTM = 11 | XINT generated when XSYNCERR is set. Interrupt on frame-synchronization error. Regardless of the value of XINTM, XSYNCERR can be read to detect this condition. For more information on using XSYNCERR, see Section 20.5.6. | |||||