SPRUJB3C March 2024 – November 2025 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
Priority tagged packets are packets that contain a VLAN header with VID = 0. According to the CPSW3_CPSW_NU_ALE_ALE_UVLAN_UNTAG[1-0] UVLAN_FORCE_UNTAGGED_EGRESS bit in the packet header, priority tagged packets may exit the switch with their VLAN ID and priority replaced or they may have their priority tag completely removed. The two cases are discussed below.
In order for a priority tagged packet to fall into this category the ENABLE_VID0_MODE bit in the CPSW3_CPSW_NU_ALE_ALE_CONTROL register must also be set to 0h. If the ENABLE_VID0_MODE bit in the CPSW3_CPSW_NU_ALE_ALE_CONTROL register is set to 1h, then packets with a VLAN VID of 0 will fall into the VLAN Tagged Packets category in Section 12.2.1.4.6.4.1.3 below.
Priority tagged input packets have the packet VLAN ID and the packet priority replaced with the header packet VLAN ID and the header packet priority when the transmit packet header CPSW_FORCE_UNTAGGED_EGRESS_REG[1-0] MASK bit is de-asserted. The header packet VLAN ID comes from the PORT_VID bits in the CPSW3_CPSW_NU_CPSW_NU_ETH_MAC_i_PN_PORT_VLAN_REG register (where N is the port where the packet entered the switch). The header packet priority is based on the packet priority to header packet priority mapping in the CPSW3_CPSW_NU_CPSW_NU_ETH_MAC_i_PN_RX_PRI_MAP_REG register (where N is the port where the packet entered the switch).
Priority tagged input packets have the 4-byte packet VLAN information removed when the transmit packet header CPSW3_CPSW_NU_ALE_ALE_UVLAN_UNTAG[1-0] UVLAN_FORCE_UNTAGGED_EGRESS bit is asserted. The 0x8100 EtherType is removed as is the two byte packet VLAN. Input 64-67 byte priority tagged packets go out with the VLAN removed and padded to 64-bytes if the PASS_CRC input bit is asserted. The input CRC bytes are used as the pad data. Input 64-byte priority-tagged packets use all four input CRC bytes as pad, input 65-byte priority-tagged packets use three of the input CRC bytes as pad, and so on. No pad is performed if the PASS_CRC input bit is not asserted - input 64-67 byte (on the wire) priority-tagged packets go out as 60-63 byte packets. The output CRC is replaced with a generated CRC when the VLAN is removed.