SPRUJB3C March 2024 – November 2025 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
The division operation is implemented to calculate 1/x followed by a multiplication with the value. The input to the LUT is 12-bit unsigned value and the output is 8-bits fraction representing 1/x calculation. The divide LUT is implemented as a non-linear ROM with 1216 (1280 for aligning to 128 size boundary) entries and up to 2 segments to reduce error. Ideally to implement a full ROM for an input space of 12 bits would require 4k entires, however to save space and reduce error, the ROM is partitioned such that it is full resolution for the first 256 entries where the curve is highly non linear, whereas the next 4k - 256 entires have a step size of 4. Each ROM entry has a bit size of 20 bits in U20Q20.
Figure 7-64 Division LUTThese are the parameters that need to be calculated based on the range of the input.
The ‘shift’ parameter at the end is a configuration register which needs to be programmed. Typical programming value is 8 to generate a result in Q12 format (such that the range is 0 to1). This is usually the case when the denominator is greater than the numerator.