SPRUJB3C March 2024 – November 2025 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
To use the stream Monitor Line and Byte counters operations:
Software should now use the interrupts in register CSIRX_MONITOR_IRQS. To be able to do that you will need to allow those interrupts through the mask register CSIRX_MONITOR_IRQS_MASK_CFG.
Note that the interrupt will trigger on each frame when it reaches byte number BYTE_COUNT in line number LINE_COUNT.
To ensure correct functionality, it is highly recommended that the input device (i.e. camera) should be configured after the CSI_RX_IF has been configured and enabled.
Software must make sure all the Virtual Channel fields in the registers explained above are set to the correct VC being used by the stream.
Figure 12-419 Line/Byte Counters Interrupt Flow Diagram