SWRU580 April 2021 CC2564C , CC2564MODA , CC2564MODN
The Headset profile (HSP) is used to connect a headset or speakerphone with a mobile device or used to connect a Audio gateway with headset device to provide basic control and voice connections. The Headset profile supports two roles, Headset and Audio Gateway. This document demonstrates how to use both roles of the profile.
It is recommended that the user visits the kit setup Getting Started Guide for MSP432 or Getting Started Guide for STM32F4 pages before trying the application described on this page.
Once the code is flashed, connect the board to a PC using a miniUSB or microUSB cable. Once connected, wait for the driver to install. It will show up as XDS110 Class Application/User UART (COM x) for MSP432, under Ports (COM & LPT) in the Device manager. Attach a Terminal program like PuTTY to the serial port x for the board. The serial parameters to use are 115200 Baud, 8, n, 1. Once connected, reset the device using Reset S3 button (For MSP432) and you should see the stack getting initialized on the terminal and the help screen will be displayed, which shows all of the commands.
Figure 8-1 HSP Demo Start Screen