SWRU580 April 2021 CC2564C , CC2564MODA , CC2564MODN
The HID Over GATT Profile (HOGP) allows a user to use HID services using Bluetooth Low Energy.
It is recommended that the user visits the kit setup Getting Started Guide page before trying the application described on this page.
Once the code is flashed, connect the board to a PC using a miniUSB or microUSB cable. Once connected, wait for the driver to install. It will show up as Tiva Virtual COM Port (COM x) or XDS110 Class Application/User UART (COM x) for MSP432 under Ports (COM & LPT) in the Device manager. Attach a Terminal program like PuTTY to the serial port x for the board. The serial parameters to use are 115200 Baud (9600 for MSP430), 8, n, 1. Once connected, reset the device using Reset S3 button and you should see the stack getting initialized on the terminal and the help screen will be displayed, which shows all of the commands.
Figure 18-1 HOGP Demo Start