SWRU580 April 2021 CC2564C , CC2564MODA , CC2564MODN
The Heart Rate profile (HRP) enables a Collector device to connect and interact with a Heart Rate sensor for use in healthcare applications. There are two roles defined in this profile. The first is the Sensor which measures the Heart Rate and the second is the collector which gets the Heart Rate and other settings from the sensor. Typically, the sensor would be present directly on the patient in a location such as the Heart or wrist measuring the temperature while the collector device is close by getting the Heart Rate from the sensor at regular intervals.
This application allows the user to use a console to use Bluetooth Low Energy (BLE) to establish connection between two BLE devices, notify the heart rate between the service and Client, get and change the location of the heart rate sensor.
It is recommended that the user visits the kit setup Getting Started Guide for MSP430, Getting Started Guide for TIVA, Getting Started Guide for MSP432 or Getting Started Guide for STM32F4 pages before trying the application described on this page.
Once the code is flashed, connect the board to a PC using a miniUSB or microUSB cable. Once connected, wait for the driver to install. It will show up as MSP-EXP430F5438 USB - Serial Port (COM x), Tiva Virtual COM Port (COM x), XDS110 Class Application/User UART (COM x) for MSP432, under Ports (COM & LPT) in the Device manager. Attach a Terminal program like PuTTY to the serial port x for the board. The serial parameters to use are 115200 Baud (9600 for MSP430), 8, n, 1. Once connected, reset the device using Reset S3 button (located next to the mini USB connector for the MSP430) and you should see the stack getting initialized on the terminal and the help screen will be displayed, which shows all of the commands.
Figure 15-1 HFP Demo StartNow connect the second board via miniUSB or microUSB cable and follow the same steps performed before within the Running the Bluetooth Code section on the first board. The second device that is connected to the computer will be the Client.