SWRU580 April 2021 CC2564C , CC2564MODA , CC2564MODN
The human interface Device enables a Host to connect and control a HID Device. There are two roles defined in this profile, Host and Device. The first is the Host which sends control and report requests and the second is the Device which responds to the Host’s requests. The Host is a Device that like a computer or tablet and the Device is a I/O Device like keyboard or mouse.
This application allows the user to use a console to use Bluetooth Low Energy (BLE) to establish connection between two BLE devices, control the Device, and get Reports and Protocols.
It is recommended that the user visits the kit setup Getting Started Guide for MSP430, Getting Started Guide for TIVA, Getting Started Guide for MSP432 or Getting Started Guide for STM32F4 pages before trying the application described on this page.
Once the code is flashed, connect the board to a PC using a miniUSB or microUSB cable. Once connected, wait for the driver to install. It will show up as MSP-EXP430F5438 USB - Serial Port(COM x), Tiva Virtual COM Port (COM x), XDS110 Class Application/User UART (COM x) for MSP432, under Ports (COM & LPT) in the Device manager. Attach a Terminal program like PuTTY to the serial port x for the board. The serial parameters to use are 115200 Baud (9600 for MSP430), 8, n, 1. Once connected, reset the Device using Reset S3 button (located next to the mini USB connector for the MSP430) and you should see the stack getting initialized on the terminal and the help screen will be displayed, which shows all of the commands.
Figure 7-1 HID Demo Start Host
Terminal